- Getting started
- Creating projects
- OPC UA
- Graphic objects
- Predefined graphic objects
- Sessions and locales
- Object and variable references
- Extending projects
- NetLogic
Align objects
Align selected objects vertically or horizontally in the Design Area. Aligning objects increases and decreases the margins of the selected items.
- InProject view, double-click a container or select.The editor opens a separate tab.
- Select the objects to align.TIP: To select multiple objects, hold downCtrland select multiple objects.
- In the Design Area toolbar, select the icon to align the selected objects in the Design Area:
Align at the left border.
Aligns at the top border.
Align at the right border.
Align at the bottom border.
Provide Feedback