- Getting started
- Creating projects
- OPC UA
- Graphic objects
- Predefined graphic objects
- Sessions and locales
- Object and variable references
- Extending projects
- NetLogic
Button
Generates events to perform methods.
Events
Use these button events to trigger methods:
Event | Generated at runtime when |
|---|---|
MouseClick event | An object is clicked or touched and then released. |
MouseDown event | An object is clicked or touched. |
MouseUp event | The click or touch of the object is released. |
Use case
Trigger different actions, for example:
- Start report generation
- Acknowledge active alarm
- Signal an emergency condition
Example
Three buttons with different styles

Provide Feedback