- Getting started
- Creating projects
- OPC UA
- Graphic objects
- Predefined graphic objects
- Sessions and locales
- Object and variable references
- Extending projects
- NetLogic
Option button
Selects a mutually exclusive option in a group.
Use case
Provide mutually exclusive options. For example, select an item from a list of alternative mechanical components or application modes.
TIP:
To create a group of mutually exclusive options, create several different
Option button
objects under a single container object.Example

Provide Feedback