- Getting started
- Creating projects
- OPC UA
- Graphic objects
- Predefined graphic objects
- Sessions and locales
- Object and variable references
- Extending projects
- NetLogic
Configure a PDF viewer
Add a PDF viewer to insert an empty container for a PDF file and then specify the PDF file to display. You can display PDF files local to the project or remote PDF files.
- InProject view, inUI, right-click a container and then select .
- InProperties, setZoom mode:
- Fit width. PDF document fits the page width.
- Fit height. PDF document fits the page height.
- Fit page. PDF document fits the page width and height.
- Actual size. Actual size of the PDF document displays in the PDF viewer container.
- Custom level. Specified zoom level of the PDF document displays in the PDF viewer container.
- InPath, either:
- SelectBrowseand select the local PDF file to display.TIP:To find items, start typing the item name to find inSelect file.If the file does not appear inSelect file, selectand inImport file(s)Import file(s), select the file to import and then chooseSelect.
- Enter the address of the remote PDF file to display.TIP:PDF viewer supports these protocols for displaying remote PDF files:
- http
- https
- (optional) To display the PDF document on a specific page, setCurrent Pageto the page to display.For example, to display the PDF document on page 5, enter5.
- (optional) Set theAppearanceandSize and layoutproperties.
Provide Feedback