- Getting started
- Creating projects
- OPC UA
- Graphic objects
- Predefined graphic objects
- Sessions and locales
- Object and variable references
- Extending projects
- NetLogic
Navigate a trend chart
Navigate the X-axis and Y-axis of a trend chart in the
Normal
trend mode.- Select a point and drag it horizontally to navigate the X-axis.TIP: If theFollowproperty is set toTrue, automatic scrolling stops when you interact with the graph. To restart the automatic scrolling of the X-axis, scroll the X-axis to the current instance.
- Select a point and drag it vertically to navigate the Y-axis.
- Select a pointer and drag it diagonally to browse on both axes.
Provide Feedback