- Getting started
- Creating projects
- OPC UA
- Graphic objects
- Predefined graphic objects
- Sessions and locales
- Object and variable references
- Extending projects
- NetLogic
Draw a rectangle or square
Use the
Rectangle
tool to draw rectangles or squares.- InProject view, double-click the container to include the object.
- In the editor toolbar, selectRectangle.
- In the editor, position the crosshair where the square or rectangle is to begin.
- Drag to draw a rectangle or square.
The object appears in the editor and in
Project view
.Provide Feedback