- Getting started
- Creating projects
- OPC UA
- Graphic objects
- Predefined graphic objects
- Sessions and locales
- Object and variable references
- Extending projects
- NetLogic
Apply a global style to the project
Select a style sheet for a
FactoryTalk Optix Application
to display at runtime.Prerequisites
- Configure a global style in a stylesheet. See Configure a style sheet.
- To apply a global style to the project
- InProject view, select eitherNativePresentationEngineorWebPresentationEngine.
- InProperties, inStyle sheet, select the drop-down arrow after the style sheet value and then select the style sheet to apply.
The project uses the
Global Style
properties from the selected style sheet.Provide Feedback