- Getting started
- Creating projects
- OPC UA
- Graphic objects
- Predefined graphic objects
- Sessions and locales
- Object and variable references
- Extending projects
- NetLogic
Import fonts
You can configure your
FactoryTalk Optix Application
to use custom fonts in TTF
or OTF
format. To use a font other than a default, import the font into the project to make it available as an object property.
TIP:
If you use folder.
FactoryTalk Optix Studio desktop editor
, instead of performing this procedure, you can copy custom TTF
or OTF
font files into the ProjectName
\ProjectFiles\Font- In the main toolbar, select.Browse project files
- InProject Files, select.Import file(s)
- Navigate to and select the font to import and then selectOpen.Verify that the font selected for the project is available on the device and supports the required characters.
- CloseProject Files.
The font is now available in the
Font family
properties of objects.Provide Feedback