- Getting started
- Creating projects
- OPC UA
- Graphic objects
- Predefined graphic objects
- Sessions and locales
- Object and variable references
- Extending projects
- NetLogic
Create a list box
Create a list box that enables you to switch between Motor and Kiln objects.
- InProject view, right-clickMainWindow (type)and select .
- InProperties, create a dynamic link betweenModeland .For more information about dynamic links, see Create dynamic links.
- ExpandModeland create a dynamic link betweenItemKindand .For more information about dynamic links, see Create dynamic links.
Provide Feedback