- Getting started
- Creating projects
- OPC UA
- Graphic objects
- Predefined graphic objects
- Sessions and locales
- Object and variable references
- Extending projects
- NetLogic
Import a template
Place a template in a node in
Project view
to add the object, object type, or a variable to the project.
TIP:
If the template is a graphic object, you can drag the graphic element from the library to the editor.
- From the main toolbar, selectand either:Template Libraries
- Drag a template from the library into a node inProject view.
- Drag a graphic object template fromLibrariesto the editor orProject view.
- If the template is an object type, select either:
- Import as type. Add an object type based on the template into the project.
- Import as instance. Add an object instance based on the template into the project.
Provide Feedback