- Getting started
- Creating projects
- OPC UA
- Graphic objects
- Predefined graphic objects
- Sessions and locales
- Object and variable references
- Extending projects
- NetLogic
Load an application
Use the Load Application Widget to load a FactoryTalk Optix Application to the device from a USB drive.
- On the device, open the screen with the Load Application Widget.
- InEnter application path, navigate to the FactoryTalk Optix Application to load from the USB drive or selectBrowseto browse for the application.
- If a password was created when the application was exported, inPassword, enter the password.
- Specify whether any existing application files on the remote device are retained or replaced:
- SelectDelete application files with updateto replace FactoryTalk Optix Application files such as the datalog if you are downloading a new FactoryTalk Optix Application.
- ClearDelete application files with updateto retain existing FacatoryTalk Optix Application files such as the datalog if you are downloading the same FactoryTalk Optix Application with only small changes or additions.
#####displays any errors or diagnostic messages that occur when the FactoryTalk Optix Application loads. - SelectLoad.
Provide Feedback