- Getting started
- Creating projects
- OPC UA
- Graphic objects
- Predefined graphic objects
- Sessions and locales
- Object and variable references
- Extending projects
- NetLogic
Logger
A logger object records data and stores it in a database.
These logger types are available:
- Data logger. Samples values of one or more variables at regular time intervals or on demand.
- Event logger. Records the properties of one or more event types generated by:
- A specific node and/or its child nodes
- Any node in the project
Provide Feedback