- Getting started
- Creating projects
- OPC UA
- Graphic objects
- Predefined graphic objects
- Sessions and locales
- Object and variable references
- Extending projects
- NetLogic
Store read operation codes
Configure the logger to store the operation codes of reading on the controller in the database.
TIP:
For more information about the read operation codes, see Read operation codes.
Prerequisites
- To store read operation codes
- InProject view, select a data logger object.
- InProperties, setLog operation code of each variabletoTrue.
Provide Feedback