- Getting started
- Creating projects
- OPC UA
- Graphic objects
- Predefined graphic objects
- Sessions and locales
- Object and variable references
- Extending projects
- NetLogic
Create a variable
Create a variable that indicates the current temperature.
- Create the variable:
- InProject view, right-clickModeland select .
- Hover-over the variable, select, and enterTemperature.
- Configure the variable:
- InProperties, selectInt32and selectFloat.
- Right-clickTemperatureand select .
- UnderEURange, setHigh limitto100.
Provide Feedback