- Getting started
- Creating projects
- OPC UA
- Graphic objects
- Predefined graphic objects
- Sessions and locales
- Object and variable references
- Extending projects
- NetLogic
Create an alarm
Create an exclusive level alarm that warns about exceeded temperature.
- InProject view, right-clickAlarmsand select .
- InProperties, setHigh limitto60.
- SetAuto confirmtoTrue
- SetMessagetoMaximum temperature exceeded
- Create a dynamic link betweenInput variableand .For more information about dynamic links, see Create dynamic links.
Provide Feedback