- Getting started
- Creating projects
- OPC UA
- Graphic objects
- Predefined graphic objects
- Sessions and locales
- Object and variable references
- Extending projects
- NetLogic
Configure the trusted certificates at design time
Set up a trusted certificate at design time by importing a file that has the certificate.
- From the toolbar, select.Browse project files
- Select a certificate and select.Import file(s)
- Select the certificate.For more information, see Certificates and keys location.
- SelectClose.
Provide Feedback