- Getting started
- Creating projects
- OPC UA
- Graphic objects
- Predefined graphic objects
- Sessions and locales
- Object and variable references
- Extending projects
- NetLogic
Configure the trusted certificates at runtime
Configure a server or client certificate rejected at runtime as a trusted certificate.
You can move the certificate in the following ways:
- Manually, by using Windows Explorer on a Windows target only.
- Remotely, by usingFactoryTalk Remote Access.
- By using the same application.
- FromApplicationFiles/PKI/Rejected, move the certificate toProjectFiles/PKI/Trusted/Certs.
After a few seconds, the certificate is considered trusted without the need to restart the
FTOptixApplications
.Provide Feedback