Import nodes from NodeSet

Import nodes from NodeSet

Import all nodes from a NodeSet
XML
file.
TIP: Import nodes from NodeSet to import all nodes from
OPC UA Companion Specifications
defined in a NodeSet file. For more information, see OPC UA Companion Specifications.
Prerequisites
Obtain an
XML
file with NodeSet to import.
  1. To import nodes from NodeSet
  2. In
    Project view
    , right-click
    Model
    folder or any of its subfolders and then select
    New
    Import from NodeSet
    .
  3. Select the
    XML
    with NodeSet to import.
The imported nodes appear in the folder.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.