- Getting started
- Creating projects
- OPC UA
- Graphic objects
- Predefined graphic objects
- Sessions and locales
- Object and variable references
- Extending projects
- NetLogic
Configure firewall for an OPC UA server
If an application has an OPC UA server running in Windows®, open the port specified in the
Endpoint URL Server
property of the OPC UA server.Prerequisites
- To configure firewall for an OPC UA server
- When running a project with an OPC UA server object, if prompted, accept requests to configure a firewall rule.
The
firewall rule is created.runtime
Provide Feedback