- Getting started
- Creating projects
- OPC UA
- Graphic objects
- Predefined graphic objects
- Sessions and locales
- Object and variable references
- Extending projects
- NetLogic
Display information model graphs
Visualize information models of
FactoryTalk Optix
projects in the form of graphs.
TIP:
For more information about project information models, see Information model.
Prerequisites
Install an application that displays graphs
DGML
graphs, such as Microsoft Visual Studio with the DGML Editor component.
TIP:
For more information about
DGML
files, see Directed Graph Markup Language (DGML) reference - Visual Studio (Windows) | Microsoft Learn.- To display information model graphs
- Do either:
- InProperties, right-click the property.
- InProject view, right-click the project node.
- SelectModel analysisand then select either:
- Information model graph (Project only). Visualize only nodes, types, and references related to the user project.
- Information model graph (Ignore OPCUA/Core namespaces). Visualize nodes, types, and references of the user project andFTOptixmodules namespaces, except OPC-UA and Core namespace.
- Information model graph. Visualize all nodes, types, and references of any namespace.
Information model graph example

Provide Feedback