Navigate nodes
Navigate project content in
Project view
.- Do any of the following:
- Select any node inProject viewand start typing the name of the node to find.The matching note is selected.TIP: The nodes are searched downward from the currently selected node. If there are no matches, the search continues from the first node to the currently selected node.
- Expand the selected node by pressing.Right arrow
- Collapse the selected node by pressing.Left arrow
- Select the lower node by pressing.Down arrow
- Select the upper node by pressing.Up arrow
- Select the previously selected node by selecting.Navigate backward
- Select the most recent node by selecting.Navigate forward
- Right-click the root project node and then selectCollapse allto collapse all nodes for easier navigation.
- DivideProject viewinto two areas that you can scroll separately. SelectSplit project viewto divide the view. SelectSplit project viewagain to remove the division in the view.
Provide Feedback