Search for nodes

Search for nodes

Use
Search
in
Project view
to search for and filter project nodes in the tree structure.
  • In
    Project view
    , perform any of the following:
    • To search for project nodes, in
      Search
      , enter a search query.
    • To clear the search query, in
      Search
      , select
      Close
      .
    • To filter project nodes by type, in
      Search
      , select
      and then select or clear the node types to include in the query.
    • To clear all filters, in
      Search
      , select
      and then select
      Clear All Filters
      .
    You can search for project nodes using their
    NodeID
    , by entering
    n:
    Node_ID
    For example:
    n: 85/00000000000123456
    TIP: You can also enter just the numeric string after the "/" as your search query. The string is unique for each project node.
    For example:
    n: 00000000000123456
    At least 4 characters of the NodeID are required to trigger the search. You can also search by
    namespace
    only, for example 
    n: 8/
    or
    n: 123/
    , with no length requirement, but this search may take more time.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.