- Getting started
- Creating projects
- OPC UA
- Graphic objects
- Predefined graphic objects
- Sessions and locales
- Object and variable references
- Extending projects
- NetLogic
View node references
View references to display all of the objects in the information model that reference a node.
- InProject view, right-click the node or item and then selectShow References.
- InReferences of (name), select a location and then selectGo to ...
FactoryTalk Optix Studio
navigates to the instance of the type. Objects referenced in a NetLogic are not shown.Provide Feedback