- Getting started
- Creating projects
- OPC UA
- Graphic objects
- Predefined graphic objects
- Sessions and locales
- Object and variable references
- Extending projects
- NetLogic
Set the unit of measure for a variable
Set the unit of measurement for a numeric figure.
- InProject view, select a variable.
- InProperties, right-click the numeric variable name and select .
- Select the unit of measure for the variable value and chooseSelect.
The unit of measure appears in the value for the variable.
Provide Feedback