Configure a recipe schema

Configure a recipe schema

Configure a recipe schema with a wizard.
  1. From the toolbar, select
    Open dashboard page
    .
  2. In the central pane, select
    Configure a recipe
    .
  3. Select an existing recipe or create a new recipe:
    • To create a recipe:
      1. Select
        New recipe
        .
      2. Edit
        Name
        .
      3. Complete
        Target node
        .
        The target node defines the recipe schema ingredients. The target node can be any project node that contains the desired variables.
        For example, the target node can be:
        • The
          Model
          folder
        • An object inside the
          Model
          folder
        • A node that contains variables from one or more controllers
        TIP: In a complex project, to define variables contained in several nodes as ingredients of a recipe schema, create a dedicated object in the
        Model
        folder and add variables inside it. Then, create a dynamic link between the variables and the ingredients. If the object is selected as the target node, the selection of the recipe schema ingredients is intuitive because only the variables referenced in the object are displayed.
      4. Select
        Next
        .
    • To edit an existing recipe:
      1. Select an existing recipe.
      2. Edit the recipe properties.
    • To duplicate an existing recipe:
      TIP: Duplicating an existing recipe enables you to create a new recipe based on the existing recipe quickly.
      1. Right-click an available recipe and select
        Duplicate
        .
      2. If needed, edit the recipe properties.
  4. Select
    Next
    .
  5. Select an existing database or configure a new database:
    • To use an existing database:
      1. Select an existing database.
      2. If necessary, edit the database properties.
      3. Select
        Next
        .
    • To create a database:
      1. Select
        New database
        .
      2. If needed, edit the
        Name
        and
        Type
        fields.
      3. Select
        Next
        .
      4. If necessary, edit the database properties.
      5. Select
        Next
        .
    • To duplicate an available database:
      TIP: Duplicating an existing database allows you to create a database base on the existing database quickly.
      1. Right-click an available database and select
        Duplicate
        .
      2. If necessary, edit the database properties.
  6. Select
    Next
    .
  7. Select the recipe parameters to use.
    TIP: You can show or hide variables (parameters) nested in other variables by using the
    Nested variables
    toggle. You can quickly find the parameters that you want to select by using the
    Search
    field.
  8. Select
    Next
    .
  9. Review the settings.
  10. Select
    Exit
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.