Reports

Reports

Use a
Reports
object to design, layout, and generate PDF reports. Reports can include data extracted from
FTOptixApplication
and databases.
Generate reports from:
  • FactoryTalk Optix Application
    to include process data and statistical data
  • A database to include data recorded by an event logger
Create a report by adding a Reports object to the project.
Apply a stylesheet to a report to customize the appearance of the report. Display information in a report footer to, for example, identify the report, page number, or other pertinent information.
To discover sample applications or report, complete the Reports tutorial.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.