Configure idle Timeout for a session

Configure idle Timeout for a session

You can use the UI Session
IdleTimeoutEvent
to have an idle timeout apply to the entire session and the Presentation Engine.
  1. In
    Project view
    , right-click the
    UI
    folder and select
    New
    UI Session
    .
    UISession# (type)
    appears in
    Project view
    .
  2. With
    UISession# (type)
    selected, in
    Properties
    , in
    Inactivity timeout duration
    , enter the duration for the timeout.
  3. In
    Inactivity timeout active
    , select
    True
    .
  4. Under
    Events
    after
    IdleTimeoutEvent
    , select
    Add
    Add new method
    , expand
    Commands
    , and navigate to select the command that will be executed when the timeout event is triggered.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.