- Getting started
- Creating projects
- OPC UA
- Graphic objects
- Predefined graphic objects
- Sessions and locales
- Object and variable references
- Extending projects
- NetLogic
Example interactive session and Presentation Engine
In this example, the start pages in the interactive sessions for
User1
, User2
, and User3
are instances of the start page set in the Presentation Engine. Each start page contains several instances of the same 
A
, B
and C
objects. The objects are shown or hidden based on the dynamic logics of each user. Text is translated based on the user locale.
Provide Feedback