Configure measurement systems map

Configure measurement systems map

Use preferred engineering units in unit systems associated with project locales. Map custom units in these systems: International System of Units, US Customary Measurement System, British Imperial Units.
TIP: The session locale determines the measurement system for the displayed data. For example, a session with the en-US locale displays temperatures in Fahrenheit degrees.
Prerequisites
(optional) Define custom engineering units. See Create an engineering units dictionary.
  1. In
    Project view
    , select the project root node.
    TIP: The root node is at the top of
    Project view
    has the same name as your project.
  2. In
    Properties
    , next to
    Measurement systems map
    , select
    Editor
    Edit with Measurement system editor
    .
  3. To add a measurement systems map row, select
    Add
    .
  4. To edit a measurement systems map row, hover-over a cell, select the drop-down arrow, and select a value.
    From
    indicates the input quantity of interest or the value from the sensor to be converted. The selected units of measure will be translated to the equivalent quantity for the different locales in these columns:
    • International System of Units
    • US Customary Measurement System
    • British Imperial Units
  5. (optional) To delete a measurement systems map row, select a cell in the measurement systems map row and select
    Delete
    .
Example: Measurement systems map
From
International System Of Units
US Customary Measurement System
British Imperial Units
Volume: liter [l]
liter [l]
quart (US) [qt (US)]
quart (UK) [qt (UK)]
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.