- Getting started
- Creating projects
- OPC UA
- Graphic objects
- Predefined graphic objects
- Sessions and locales
- Object and variable references
- Extending projects
- NetLogic
Develop a persistent setting specific to a user
Create a checkbox that shows or hides a clock label, which state is persistent based on the currently logged in user.
Application example

NOTE:
Download a sample project:
UserSpecificPersistentSetting.zipPrerequisites
- To develop the project
- Arrange the interface elements.
- Save the project.
Application design example

Select
to run the project using the client emulator to test your project. To run the project on a remote client, see Add a client device.
Run
Provide Feedback