- Getting started
- Creating projects
- OPC UA
- Graphic objects
- Predefined graphic objects
- Sessions and locales
- Object and variable references
- Extending projects
- NetLogic
View alarms in remote local time zone
View alarms in the local time zone to view alarm events remotely.
- Select.Template Libraries
- InTemplate Libraries, drag theAlarm gridorAlarm history gridobject fromWidgetsinto a node in theUIfolder.
- InProject view, select the alarm object.
- InProperties, expandTimestamp.
- InText, reset the current value and then select.Change Dynamic Link
- At the bottom of the window, selectAdvanced...
- In the Advanced Dynamic Link editor, selectInsertand then selectExpression evaluator.
- InExpression, enter{0} + {1}
- In the{0} DynamicLinkpane, selectand then select .Change Dynamic Link
- In{1} DynamicLink, selectand then select .Change Dynamic Link
- ChooseSelect.
Provide Feedback