- Getting started
- Creating projects
- OPC UA
- Graphic objects
- Predefined graphic objects
- Sessions and locales
- Object and variable references
- Extending projects
- NetLogic
Change the interface language
Change the interface language to display a different language throughout the
FactoryTalk Optix Studio
application at design time and runtime. - To change the interface language, either:
- InProject view, select the project node and then inProperties, expandLocalizationand inLocales, select the language.
- Selectand then inFactoryTalk Optix Studio OptionsLanguage and Locale, select the language.
- Have a different user with a different associated locale language log on.
Provide Feedback