- Getting started
- Creating projects
- OPC UA
- Graphic objects
- Predefined graphic objects
- Sessions and locales
- Object and variable references
- Extending projects
- NetLogic
Assign a role to a user or group
Assign roles to users and groups to create a hierarchy roles with assigned rights and privileges.
- In the main toolbar, selectand then selectOpen dashboard pageManage users and groups.
- On the dashboard page, either:
- UnderRoles,drag a group onto a user underUsersor onto a group underGroups. You can also drag a user or group onto a role. Hold downShiftorCtrlto select and drag consecutive or multiple selections.
- Select one or more roles, selectAssignroles to users or groups, select the users and groups, and then selectApply.
- SelectExit.NOTE:
appears next to a group or role that is already assigned to a role. You can assign the role to a user or group from
Project viewby dragging the role to the user or group inProject view.NOTE: To assign a role from a context menu, inManage users and groups, right-click the role, selectAssign to users or groups, select the roles to assign to the user or group, and then selectApply. - SelectExit.
The role appears assigned to the user or group on the dashboard page.
Provide Feedback