- Getting started
- Creating projects
- OPC UA
- Graphic objects
- Predefined graphic objects
- Sessions and locales
- Object and variable references
- Extending projects
- NetLogic
Delete a role
Delete a role to remove the role and no longer have the assigned users be members of the role.
Delete a role from either the dashboard page or
Project view
.- In the main toolbar, selectand then selectOpen dashboard pageManage users and groups.
- On the dashboard page underRoles, select the role or roles to delete.
- SelectDelete.TIP: You can also right-click the role to delete on either the dashboard page or inProject viewand then selectDelete.
Provide Feedback