Rename a user
Rename a user to change the name of the user in the project and in groups. You can rename one user at a time.
Rename a user from either the dashboard or
Project view
.- Either:
- In the main toolbar, select, and then selectOpen dashboard pageManage user and groups.
- InProject view, expandSecurityandUsers.
- UnderUsers, right-click the user to rename.
- SelectRenameand enter a new name.NOTE: To rename a user fromProject view, right-click the user, selectRename, and then enter the new name.
The user is renamed on the dashboard and in
Project view
. Provide Feedback