- Getting started
- Creating projects
- OPC UA
- Graphic objects
- Predefined graphic objects
- Sessions and locales
- Object and variable references
- Extending projects
- NetLogic
Manage dynamic links
Use C# APIs to set or remove dynamic links on the variables.
The APIs are supplied by the
IUAVariable
C# class.
TIP:
By default, dynamic links defined in a NetLogic are read-only, whereas dynamic links created with the
FactoryTalk Optix Studio
UI are read and write.Provide Feedback