- Getting started
- Creating projects
- OPC UA
- Graphic objects
- Predefined graphic objects
- Sessions and locales
- Object and variable references
- Extending projects
- NetLogic
Set the default code editor
We recommend using Microsoft Visual Studio 2022 or Microsoft Visual Studio Code as the default code editor.
TIP:
Some development assistance features may not be available when using a different code editor.
Prerequisites
Download and install the preferred code editor.
- To set the default code editor
- InFactoryTalk Optix Studio, select.FactoryTalk Optix Studio Options
- In the dialog, from thePreferred code editordrop-down menu, select an option.TIP: TheAutomaticoption sets Visual Studio as the default editor. If Visual Studio is not available, Visual Studio Code is used as the default editor instead.
- RestartFactoryTalk Optix Studio.
Provide Feedback