- Getting started
- Creating projects
- OPC UA
- Graphic objects
- Predefined graphic objects
- Sessions and locales
- Object and variable references
- Extending projects
- NetLogic
Project view
Project view
displays the contents of the FactoryTalk Optix Application
in a tree structure of folders.Folders
Each folder has a dedicated icon and context menu. The context menu displays objects that you can create in that folder. Any subfolder that you create displays the same options as the folder on which it is based. You can create multiple versions of a folder.
Buttons
Project view
contains buttons for navigating the contents of the application. Some buttons appear on either the title bar of Project view
or in the selected object.
Item | Description |
---|---|
![]() Navigate backward | Set focus on the previously selected pane. |
![]() Navigate forward | Set focus on the next selected pane. |
![]() Split project view | Divide Project view into two panes. |
![]() Add new | Create a node inside the selected node. |
Delete | Remove the selected node and the nodes that it contains. |
![]() Detach view | Detach the pane from the main window. |
![]() Attach view | Detach the pane to the main window. |
![]() Lock | Lock the selected child node to hide it from Project view . You cannot edit locked child nodes. |
![]() Unlock | Unlock the selected child nodes to display it in Project view . You can edit unlocked child nodes. |
![]() Unlock | Open the selected object in the dedicated editor. Only certain object types have a dedicated editor. |
Search bar
Use
Search
in Project view
to search for and filter project nodes in the tree structure.Item | Description |
---|---|
Search | Filters the project nodes in the tree structure based on the search query. |
![]() | Displays if you enter a search query. Select to clear the search query. |
![]() | Expands the available filters picker. |
![]() | Collapses the available filters picker. |
![]() | Indicates active filters. Expand or collapse the available filters picker. |
Provide Feedback