- Getting started
- Creating projects
- OPC UA
- Graphic objects
- Predefined graphic objects
- Sessions and locales
- Object and variable references
- Extending projects
- NetLogic
Configure a digital alarm
Configure a simple Boolean alarm that warns you about issues with Motor1 at runtime.
TIP:
By default, a digital alarm triggers when its
Input variable
equals to 1. For more information, see Alarm types.- InProject view, right-clickAlarmsand select .
- InProperties, create a dynamic link between theInput variableandMotor1Alarmvariable.For more information about dynamic links, see Create dynamic links.
- InMessage, enter a warning message.For example, enterMotor1 alarm.
Provide Feedback