- Getting started
- Creating projects
- OPC UA
- Graphic objects
- Predefined graphic objects
- Sessions and locales
- Object and variable references
- Extending projects
- NetLogic
Associate the LED status with the switch
Turn the LED object on and off with the switch.
- InProject view, selectLED1.
- InProperties, create a dynamic link betweenActiveand .For more information about dynamic links, see Create dynamic links.
LED toggle


Provide Feedback