- Getting started
- Creating projects
- OPC UA
- Graphic objects
- Predefined graphic objects
- Sessions and locales
- Object and variable references
- Extending projects
- NetLogic
Automatically confirm and acknowledge alarms
Reduce the interaction required to manage alarms at runtime. Have the application confirm and acknowledge alarms automatically.
- InProject view, select theAlarm grid.
- InProperties, configure:
- Auto confirm. SelectTrueto confirm that the issues causing alarms are resolved at runtime automatically. TheAlarm griddisplays only active and unacknowledged alarms.
- Auto acknowledge. SelectTrueto acknowledge alarms at runtime automatically. TheAlarm griddisplays only unacknowledged alarms.TIP: To have theAlarm griddisplay only active alarms at runtime, inPropertiesfor the grid, set bothAuto confirmandAuto acknowledgetoTrue.
Provide Feedback