- Getting started
- Creating projects
- OPC UA
- Graphic objects
- Predefined graphic objects
- Sessions and locales
- Object and variable references
- Extending projects
- NetLogic
Translate an alarm message
The message displayed in an
Alarms
widget is a text string that can appear in different languages. Enter a message, select the language for the translation, and then enter the translated string. The translated alarm message appears in the language of the user at runtime.Prerequisites
- To translate an alarm message
- InProject view, navigate to and select the alarm.
- InProperties, inMessage, type the message the alarm event is to display at runtime.
- InProject view, expandTranslations.
- Double-clickLocalizationDictionary#
- In the Translation Editor, selectViewTranslation Reference.Your new message appears in theStringcolumn.
- In the row of the alarm message, selectSynchronize.A corresponding translated message appears in theKeycolumn.
- SelectView Translation Table.
- SelectAdd locale, select the desired language for the translation, and then select.
- InNew locales added, selectYes.
- In the third column, enter the string for the translation.
Provide Feedback