- Getting started
- Creating projects
- OPC UA
- Graphic objects
- Predefined graphic objects
- Sessions and locales
- Object and variable references
- Extending projects
- NetLogic
Create a motor values widget instance
Create a motor values widget instance from the motor values widget type.
- InProject view, right-clickMainWindow (type)and select .
- InProperties, create a dynamic link betweenMotorand .For more information about dynamic links, see Create dynamic links.
Provide Feedback