- Getting started
- Creating projects
- OPC UA
- Graphic objects
- Predefined graphic objects
- Sessions and locales
- Object and variable references
- Extending projects
- NetLogic
Create an acceleration gauge and labels
- Create the speed gauge:
- InProject view, right-clickMotorAccelerationPaneland select .
- Hover-over the gauge, select, and enterAccelerationGauge.
- InProperties, create a dynamic link betweenValueand .For more information about dynamic links, see Create dynamic links.
- Create the speed label:
- InProject view, right-clickMotorAccelerationPaneland select .
- Hover-over the label, select, and enterAccelerationLabel.
- InProperties, setTexttoAcceleration.
- Create the speed value label:
- InProject view, right-clickMotorAccelerationPaneland select .
- Hover-over the label, select, and enterAccelerationValueLabel.
- InProperties, create a dynamic link betweenTextand .For more information about dynamic links, see Create dynamic links.
Provide Feedback