Dynamic link browser

Dynamic link browser

Use the dynamic link browser to select the source node or attribute of the link from the information model of the project.
The content of the dynamic link browser depends on the data type of the variable that opened the browser, as well as the variable selected in the browser. For example, the
Format
options appear only if the variable that opens the browser has a String of LocalizedText data type. No other data types display the
Format
option.
Open the dynamic link browser by selecting
Add Dynamic Link
or
Change Dynamic Link
.
Item
Name
Description
1
Basic
Display the project nodes that you can use to create a dynamic link. This tab is disabled for complex dynamic links.
2
Advanced
Display the complex dynamic link editor in the dynamic link browser. See Complex dynamic link editor.
3
Filter nodes.
4
Path
Target of the selected variable.
5
Search
Search for nodes.
6
Project
Browse through the project information model.
7
Attribute
OPC UA attribute to apply to the selected node.
8
Format
Format to apply to the selected variable.
9
Array indexes
Array index of the selected variable. This option appears for array variables only.
10
Bit index
Index to access the specified bit of the selected variable.
11
Cancel
Cancel the creation of the dynamic link. Instead of selecting
Cancel
, you can select a blank area outside the dynamic link browser.
12
Select
Create a dynamic link with the selected object.
13
Remove link
Remove the dynamic link. In the event that the dynamic link cannot be removed,
Restore link
appears.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal