Edit a dynamic link
Edit a dynamic link to change the source variable or resolve a broken or unresolved link. Insert a placeholder such as {0} to make the link dynamic. Broken links display
in the property while unresolved links display
. Unresolved dynamic links cannot be resolved at design time, but they can be valid at runtime, for example, when setting a dynamic link that passes through a panel loader.


Edit a dynamic link by either editing the link manually, selecting a new source, or dragging a new source to the dynamic link in
Properties
.- To edit the dynamic link manually:
- InProperties, hover over a dynamic link and select.
- Edit the path and then press.EnterTIP: You can edit Alias indexes.
- To edit the dynamic link by selecting a new source:
- InProperties, in the property with the dynamic link, select either the link in the property or select.Change Dynamic Link
- In the dynamic link browser, select a node to act as the source of the value property.
- (optional) InAttribute, select the OPC UA attribute to apply to the selected node. For example, selectBrowseName,Value, orDisplayName.
- (optional) InFormat, select the format to apply to the selected variable.
- (optional) InArray index, select the array index of the selected variable. This option appears for array variables only.
- InBit index, select the index to access the specified bit of the selected variable.
- (optional) To create a complex dynamic link, selectAdvanced.NOTE: For more information, see Create a complex dynamic link.
- ChooseSelect.
- To edit the dynamic link by dragging a new source, drag the new source onto the existing dynamic link inProperties.
- To restore a dynamic link for which you have selected the variable, right-click the property value and then selectRestore link.
Provide Feedback