Global methods for nodes
Use these global methods to create or remove objects and variables from the information model at runtime.
CreateObject method
This method adds an object to the information model.
Argument | Description |
---|---|
BrowseName | Name of the object |
ObjectType | Type of object |
ParentNode | Parent node of the object to be created |
ReferenceType | Reserved for future use |
Argument | Description |
---|---|
CreateNodeId | NodeId attribute assigned at runtime |
CreateVariable method
This method creates a variable in the information model.
Argument | Description |
---|---|
BrowseName | Variable name |
RequestedNodeId | Reserved for future use |
VariableType | Type of variable |
ParentNode | Parent node of the variable to be created |
ReferenceType | Reserved for future use |
DeleteNode method
This method deletes a node from the information model.
Argument | Description |
---|---|
Node | Node to delete |
Provide Feedback