- Getting started
- Creating projects
- OPC UA
- Graphic objects
- Predefined graphic objects
- Sessions and locales
- Object and variable references
- Extending projects
- NetLogic
Change objects order
Move selected objects in front of or behind other objects in the editor.
- InProject view, double-click a container or select.The editor opens a separate tab.
- Select the object to move.TIP: To select multiple objects, holdCtrland select multiple objects.
- In the editor toolbar, select the button to move the object in relation to other objects:
- Send to back. Send the object behind all objects in the editor.
- Send backward. Send the object behind the next object in the editor.
- Bring forward. Send the object in front of the next object in the editor.
- Bring to front. Send the object in front of all objects in the editor.
Provide Feedback