- Getting started
- Creating projects
- OPC UA
- Graphic objects
- Predefined graphic objects
- Sessions and locales
- Object and variable references
- Extending projects
- NetLogic
Animate a graphic object
Add and configure number, sequential, or parallel animation properties to animate an object.
- InProject view, select the object to animate.
- InProperties, at the top, selectand then select either:
- Number animation. Animate objects by changing the value to another value over specific time.
- Sequential animation. Animate objects with a simple transition in the serial mode.
- Parallel animation. Animate object with a simple transition in the parallel mode.
TIP: You can also right-click a property that supports animations and select. - Configure animation properties. See Animation properties.
Provide Feedback