- Getting started
- Creating projects
- OPC UA
- Graphic objects
- Predefined graphic objects
- Sessions and locales
- Object and variable references
- Extending projects
- NetLogic
Linear gauge
Sets or displays an integer value within a range of possible values.
Use case
Set or display the value of an analog variable within a minimum and maximum value.
TIP:
Use the
Tooltip
property to show or hide the display of the value above the selection point on the gauge. Use the Warning zone
property to display specific ranges of values in different colors.Example
Linear gauge with two warning zones defined

Provide Feedback